问答
讨论
文档
Members
Tags
Cancel
常见问题
马上提问
Open Questions. Can you
help
?
4线DIA的数据问题
Not Answered
3 months ago
请教MAX30009阻抗计算
Not Answered
3 months ago
该专区内容有关生物/电化学/磁场/温度传感器专区的讨论和常见问题解答。 发帖前请阅读 Analog Devices EngineerZone 行为准则。
All Threads
by
kehm
生物/电化学/磁场/温度传感器专区
Latest
3 months ago
by
kehm
497
5
1
Not Answered
4线DIA的数据问题
0
Not Answered
我已经成功与ad5941建立了通信,使用了AD5940_BIA中的例程,现在将测量端子放置在50k的定值电阻上,并不能量出正确的值。附上采集数据图,绿色为频率,红色为实部,蓝色为虚部。以及原理图 观察到一个现象,将s+(AIN2)放置于电阻同一侧时,产生的激励波形消失了(示波器观察)。这是正常的吗
BIA
software
ad5941
A/D and D/A Converter Combinations
Analog Temperature Sensors
ad594
Temperature Sensor and Control Devices
ad5940
Show More
497
5
1
by
maomao190
生物/电化学/磁场/温度传感器专区
Latest
3 months ago
by
ADIYX
367
2
0
Not Answered
请教MAX30009阻抗计算
0
Not Answered
请教关于MAX30009校准流程,手册上校准第一步是如下图,请问框出来的电阻应该怎么计算得到? 按照下面的计算公式对吗? 其中Iadc是I通道ADC值,Zi是文档里面说的I通道的电阻值吗? double mag =Iadc; double current = 32E-6; //this depends on setting double p = pow(2,19)*1*(2/3.14)*(current); double ZI = mag/p; 请问有阻抗计算的参考程序吗...
Biopotential Sensors
software
Bio-Sensors
MAX30009
367
2
0
by
tongtongsakura
生物/电化学/磁场/温度传感器专区
Latest
4 months ago
by
ADIYX
819
4
0
Answered
MAX30009上位机是如何换算阻抗值?
0
Answered
各位好, 最近我在使用max30009的评估板进行4线法阻抗测量测试时,发现参考应用手册的标定方法无法计算出有效的阻抗模值,但是上位机显示是正确的。 但是,我将测试的数据导出来之后,参考手册的计算方式进行计算;使用1K的电阻进行外部校准,校准参数如下图所示 计算出来的阻抗模值并不是510Ω,而是77100这样的数据,请问这是什么原因导致的?
Biopotential Sensors
Bio-Sensors
MAX30009
819
4
0
by
NCU
生物/电化学/磁场/温度传感器专区
Latest
4 months ago
by
ADIYX
590
3
0
Answered
MAX30009 電路布局
0
Answered
我在看 MAX30009 的 EVB 版圖時,發現內層的鋪銅被移除得蠻多的。 從第二層開始,基本上只有輸入端附近還有鋪銅;第三層挖得更大;到第四層幾乎只剩走線,幾乎沒有整片鋪銅,等於在多個內層挖出一大塊空區。 以混合訊號或低振幅類比電路的角度來看,這樣拿掉參考平面通常會讓回流路徑變差、抗雜訊能力下降,所以有點好奇這樣設計的用意。 這樣做主要是為了降低生物阻抗輸入端的寄生電容、漏電或基板耦合嗎?還是說這個 EVB 的版圖本來就是偏向量測與特性驗證,而不是量產最佳化? 如果自己畫板的話...
Biopotential Sensors
hardware
pcb
layout
鋪銅
Bio-Sensors
MAX30009
Show More
590
3
0
by
NCU
生物/电化学/磁场/温度传感器专区
Latest
4 months ago
by
ADIYX
335
1
0
Answered
MAX30009 layout
0
Answered
I’m reviewing the MAX30009 EVB layout and noticed an aggressive copper removal strategy in the inner layers. From Layer 2 onward, copper is only kept near the input area. Layer 3 has even larger clearances, and on Layer 4 there is almost no copper pour...
Biopotential Sensors
hardware
Bio-Sensors
MAX30009
335
1
0
by
SWang929
生物/电化学/磁场/温度传感器专区
Latest
4 months ago
by
ADIYX
254
1
0
Answered
3 導程(Lead I, Lead II, Lead III)量測
0
Answered
MAX30001可以用來做3導程(Lead I, Lead II, Lead III )量測嗎? 如果可以,需要如何設計? 或者有其他推薦元件可以用來做3導程的量測?
Biopotential Sensors
hardware
MAX30001
Bio-Sensors
254
1
0
by
lzw
生物/电化学/磁场/温度传感器专区
Latest
5 months ago
by
ADIYX
301
1
0
Answered
MAX30009EVKIT测量阻抗体积描记(IPG)不稳定
0
Answered
有没有人遇到过使用MAX30009EVKIT测量阻抗体积描记(IPG)时信号不稳定?对同一个人测量,有时信号非常好,有时又噪声大到无法看出心跳波形。
Biopotential Sensors
hardware
MAX30009EVKIT
Bio-Sensors
MAX30009
Show More
301
1
0
by
gimmyhuang
生物/电化学/磁场/温度传感器专区
Latest
5 months ago
by
JimHuang
567
4
0
Discussion
maxm86161
Discussion
我们使用MAXM86161的时候遇到了一个问题,我们的IIC总线上挂载了三个芯片,目前只有MAXM86161无法通信,IIC总线速率为100K,EN引脚测试为3.3V,芯片供电测试为3.3V,IIC总线上发送指令后设备未响应,能帮忙排查一下问题吗?
MAXM86161
software
sensors
Optical Sensing Technology
Sensors and MEMS
Show More
567
4
0
by
wwwwwqq
生物/电化学/磁场/温度传感器专区
Latest
6 months ago
by
ADIYX
403
3
0
Answered
cn0565esp32s3adu3029adu3029
0
Answered
您好,我想在cn0565设备中可以使用esp32s3芯片替换调adu3029开发板,如果可以的话,那adu3029开发板上面的板子引脚都是什么功能呢,应该怎么连接呢,十分感谢!
hardware
CN0565
403
3
0
by
MAK0815
生物/电化学/磁场/温度传感器专区
Latest
6 months ago
by
MAK0815
1053
7
0
Answered
MAX31856过压/欠压故障无法解决
0
Answered
我设计制作了一个32路的测温模块( 13脚改成了悬空 ),这边在测试在一个工业管道内的安装的金属板, MAX31856连接电焊在金属板上的热电偶(或者接触公司有一个电烙铁的尖端),会出现过压/欠压故障 ,导致芯片强制停止转化,MCU读取那个通道温度卡死 我使用示波器测试一个通道(只能使用电烙铁复现,去工业管道那里测试比较麻烦),探头一边接地,一边接触T-/T+。悬空时有一个200mv左右的直流电压,接触电烙铁尖端时,测试的直流信号被拉到0V附近(最小值有-220mv左右),同时 MCU通过485转USB到电脑...
Digital Temperature Sensors
hardware
sensors
Integrated/Special Purpose A/D Converters
MAX31856
Show More
1053
7
0
View All Threads
by
NCU
生物/电化学/磁场/温度传感器专区
Latest
4 months ago
by
ADIYX
590
3
0
Answered
MAX30009 電路布局
0
Answered
我在看 MAX30009 的 EVB 版圖時,發現內層的鋪銅被移除得蠻多的。 從第二層開始,基本上只有輸入端附近還有鋪銅;第三層挖得更大;到第四層幾乎只剩走線,幾乎沒有整片鋪銅,等於在多個內層挖出一大塊空區。 以混合訊號或低振幅類比電路的角度來看,這樣拿掉參考平面通常會讓回流路徑變差、抗雜訊能力下降,所以有點好奇這樣設計的用意。 這樣做主要是為了降低生物阻抗輸入端的寄生電容、漏電或基板耦合嗎?還是說這個 EVB 的版圖本來就是偏向量測與特性驗證,而不是量產最佳化? 如果自己畫板的話...
Biopotential Sensors
hardware
pcb
layout
鋪銅
Bio-Sensors
MAX30009
Show More
590
3
0
by
NCU
生物/电化学/磁场/温度传感器专区
Latest
4 months ago
by
ADIYX
335
1
0
Answered
MAX30009 layout
0
Answered
I’m reviewing the MAX30009 EVB layout and noticed an aggressive copper removal strategy in the inner layers. From Layer 2 onward, copper is only kept near the input area. Layer 3 has even larger clearances, and on Layer 4 there is almost no copper pour...
Biopotential Sensors
hardware
Bio-Sensors
MAX30009
335
1
0
by
SWang929
生物/电化学/磁场/温度传感器专区
Latest
4 months ago
by
ADIYX
254
1
0
Answered
3 導程(Lead I, Lead II, Lead III)量測
0
Answered
MAX30001可以用來做3導程(Lead I, Lead II, Lead III )量測嗎? 如果可以,需要如何設計? 或者有其他推薦元件可以用來做3導程的量測?
Biopotential Sensors
hardware
MAX30001
Bio-Sensors
254
1
0
by
lzw
生物/电化学/磁场/温度传感器专区
Latest
5 months ago
by
ADIYX
301
1
0
Answered
MAX30009EVKIT测量阻抗体积描记(IPG)不稳定
0
Answered
有没有人遇到过使用MAX30009EVKIT测量阻抗体积描记(IPG)时信号不稳定?对同一个人测量,有时信号非常好,有时又噪声大到无法看出心跳波形。
Biopotential Sensors
hardware
MAX30009EVKIT
Bio-Sensors
MAX30009
Show More
301
1
0
by
gimmyhuang
生物/电化学/磁场/温度传感器专区
Latest
5 months ago
by
JimHuang
567
4
0
Discussion
maxm86161
Discussion
我们使用MAXM86161的时候遇到了一个问题,我们的IIC总线上挂载了三个芯片,目前只有MAXM86161无法通信,IIC总线速率为100K,EN引脚测试为3.3V,芯片供电测试为3.3V,IIC总线上发送指令后设备未响应,能帮忙排查一下问题吗?
MAXM86161
software
sensors
Optical Sensing Technology
Sensors and MEMS
Show More
567
4
0
by
tongtongsakura
生物/电化学/磁场/温度传感器专区
Latest
4 months ago
by
ADIYX
819
4
0
Answered
MAX30009上位机是如何换算阻抗值?
0
Answered
各位好, 最近我在使用max30009的评估板进行4线法阻抗测量测试时,发现参考应用手册的标定方法无法计算出有效的阻抗模值,但是上位机显示是正确的。 但是,我将测试的数据导出来之后,参考手册的计算方式进行计算;使用1K的电阻进行外部校准,校准参数如下图所示 计算出来的阻抗模值并不是510Ω,而是77100这样的数据,请问这是什么原因导致的?
Biopotential Sensors
Bio-Sensors
MAX30009
819
4
0
by
MAK0815
生物/电化学/磁场/温度传感器专区
Latest
6 months ago
by
MAK0815
1053
7
0
Answered
MAX31856过压/欠压故障无法解决
0
Answered
我设计制作了一个32路的测温模块( 13脚改成了悬空 ),这边在测试在一个工业管道内的安装的金属板, MAX31856连接电焊在金属板上的热电偶(或者接触公司有一个电烙铁的尖端),会出现过压/欠压故障 ,导致芯片强制停止转化,MCU读取那个通道温度卡死 我使用示波器测试一个通道(只能使用电烙铁复现,去工业管道那里测试比较麻烦),探头一边接地,一边接触T-/T+。悬空时有一个200mv左右的直流电压,接触电烙铁尖端时,测试的直流信号被拉到0V附近(最小值有-220mv左右),同时 MCU通过485转USB到电脑...
Digital Temperature Sensors
hardware
sensors
Integrated/Special Purpose A/D Converters
MAX31856
Show More
1053
7
0
by
supermouthhero
生物/电化学/磁场/温度传感器专区
Latest
7 months ago
by
ADIYX
409
1
2
Answered
AD5941与nrf52832的数据传输问题
0
Answered
使用AD5941自带的Ramp例程采集数据,随后将采集到的数据通过SPI通信传输给nrf52832。我们根据官方提供的代码移植方式进行了移植,使用提供的SPI例程可以成功读取到器件ID,但使用Ramp例程后nrf52832从SPI读取的数据一直是同一个不变的值。我想知道问题大概出现的哪里?有什么方式可以快速的排查出问题在哪? SPI_RAMP.rar
software
ad5941
sensors
Sensors and MEMS
Electrochemical Sensors
Show More
409
1
2
by
suishilong
生物/电化学/磁场/温度传感器专区
Latest
7 months ago
by
ADIYX
387
2
0
Answered
MAX30105停产了吗
0
Answered
MAX30105停产了吗? 有替代方案吗
hardware
product
MAX30105
387
2
0
by
wwwwwqq
生物/电化学/磁场/温度传感器专区
Latest
6 months ago
by
ADIYX
403
3
0
Answered
cn0565esp32s3adu3029adu3029
0
Answered
您好,我想在cn0565设备中可以使用esp32s3芯片替换调adu3029开发板,如果可以的话,那adu3029开发板上面的板子引脚都是什么功能呢,应该怎么连接呢,十分感谢!
hardware
CN0565
403
3
0
View All Threads
更多内容
Post
Go back to editing
Filter
Show More