Post Go back to editing

A2B MIC TESTING SYSTEM

Thread Summary

The user wants to design a 6 A2B MICs (AD2427) testing system with one A2B master node. The final answer suggests using AD2428 as the main node instead, as AD2427 only supports PDM and not TDM/I2S. A 3 Node Sample Demo of AD2428 is available for reference, and the part numbers of sub nodes can be updated to AD2427 in Sigma Studio. The A2B Software Package for Windows/Baremetal Previous Release (SigmaStudio) includes a demo quick start guide under the installation path.
AI Generated Content

I want design one 6 A2B MICs(AD2427)  testing system , let one A2B master (AD2427) node and 6 A2B MIC slave node in A2B net, How to config the A2b Master node system and can get every MIC audio output signal .  is there any example or config file for reference ?

Parents
  • Hi, Alex,

    Thank you for reaching out.

    I should first clarify that AD2427 just support sub node capable device only and support PDM and no TDM/I2S support. Therefore, you may use AD2428 as main node instead.

    There is a 3 Node Sample Demo of AD2428 for your reference. You can update the part number of sub nodes in Sigma Studio (SS)'s schematic from AD2428 to AD2427. 

    You should first download A2B Software Package as follow. 

    A2B Software for Windows/Baremetal Previous Release (SigmaStudio)

    Under the installation path, you can find the demo quick start guide at

    <Your installation path>\Analog Devices\ADI_A2B_Software-Rel19.4.4\Docs

  • Hi , Thank you for your answer , 

    Yes,  we use the 3 node sample demo from the installation package , also modify the main node chip to 2428, and sub nodes is 2427,  but we find one issue , we only can get the last node signal , and can not get the others node signal , what is the issue  and how to solve ? can you send me one config file ? alexhe@issauto.com,  thank you,

    Alex

  • Hi, Alex,

    Thank you for reply. 

    Sorry for late response. Since you are debugging with the 3 node sample demo, may I ask if the problem you met is that you can only hear the headphone input from the last node but cannot hear the microphone input from the mid sub node? If you wish to use digital microphone input, you should enable the Alt. Clock on IO7  configuration.

    Should you have any further questions, please feel free to reply.

Reply
  • Hi, Alex,

    Thank you for reply. 

    Sorry for late response. Since you are debugging with the 3 node sample demo, may I ask if the problem you met is that you can only hear the headphone input from the last node but cannot hear the microphone input from the mid sub node? If you wish to use digital microphone input, you should enable the Alt. Clock on IO7  configuration.

    Should you have any further questions, please feel free to reply.

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.