Post Go back to editing

ADSP21571启动异常

我们在使用21571芯片的过程中出现过个别案例,Dsp芯片异常,无法启动,下电后重启不恢复。具体表现如下:

1、DSP不能通过ICE1000刷写软件
2、DSP可以通过debug方式,访问flash
3、上电时,DSP与flash之间,DSP没有拉flash片选信号,没有给flash时钟信号,这个是DSP片内ROM程序异常

4、问题件的Dsp 1V1以及3V3供电电压正常,晶振正常,Reset信号正常;
5、DSP与外挂Flash之间无数据交互;
6、DSP没有给外挂Flash发出片选信号;

7、寄存器正常板子与错误板子对比,RCU0_MSG.ERRCODE,问题板子值为17,正常板子值为0

8、异常板子PC指针跳转地址,与正常板子跳转地址不一致