问题: adf7020收发

你好,各位专家,我在调试7020时,采用的是GFSK调制,我想问一下,数据时钟收发是否都是由7020提供,还是收是7020提供,发由单片机提供,我采用的是IO模拟收发数据,及提供时钟,另外在同步检测时也未检测到INT引脚电压变高,未同步,不知道收数据时前导字要不要检测判断。

  • 您好!根据数据手册中描述,在GFSK模式,数据时钟由DATA CLK输出。 In receive mode, the pin outputs the synchronized data clock. The positive clock edge is matched to the center of the received data. In GFSK transmit mode, the pin outputs an accurate clock to latch the data from the microcontroller into the transmit section at the exact required data rate. See the Gaussian Frequency Shift Keying (GFSK) section.

  • 在设置为GFSK模式后,我从data_clk看到波形了。应该就是从7020输出的。我想问一下,如果采用外部的收发开关,代替内部的收发开关,请问该如何设置,是不是将寄存器8中的D8_12的Tx/Rx Switch 设置为1就ok了?还是有其他的设置?自己一直在摸索着,最近在出差中,也没有机会调试,谢谢专家的指导。同步这一块我还没有调通。

  • 0
    •  Analog Employees 
    on Apr 29, 2019 10:32 AM
    This question has been closed by the EZ team and is assumed answered.