最爱ADI放大器之- AD712 by huangguimin
我最喜欢的ADI放大器AD712是一款双通道、高速、精密、单芯片运算放大器,具有极高的性价比。我是玩音响的,也就是玩HIFI的,我用这颗运放作为整个HIFI功放的输入前端,也就是前级。运放对选型对整个功放的素质影响很大,不同的运放能产生天壤之别的音质差异。对这颗运放比较熟悉,整体来说AD712是不错的运放!属于监听级的类型。特显中频与高频之间的过度交替。声场比较广!低音稍少!高音稍粗(相对高级的)低噪音很静没有半点杂音。听纯音乐女声不错属于比较耐听的运放之一!由于我只买到kn塑封。陶封找来找去都无得卖!听说陶封的效果还好点!用户可以轻松升级采用旧型号精密BiFET的现有设计。这款运算放大器具有出色的交流和直流性能,适合有源滤波器应用。因而AD712非常适合用作12位DAC/ADC的缓冲器以及高速积分器。同时,建立时间性能则是任何类似IC放大器所无法比拟的。使用在HIFI功放上是当之无愧的!