Post Go back to editing

ad8676对5V电压基准放大至10V多次烧毁

我按照UG-184(AD5781DAC参考电路)搭建了反比例放大电路,实现对5V电压基准放大至-10V,在PCB板上芯片内一运放电路实现电压跟随阻抗匹配功能工作正常输出5V,另一个运放出现烧毁输出13V之多,第二块在PCB板上出现了烧毁,第三块使用面包板进行测试也出现烧毁,且导致线性电源的CH4(提供5V模拟基准电压)毁坏。电源供电采用线性电源正负15V供电,电源CH2的+与电源GND相连并且也是运放的地,CH2的-作为-15V;CH1的正作为+15V,-与运放地、电源地GND、CH2正连通;CH3+作为信号输出,CH3的-与前述的地相连。这个连接方式在我使用两个运算放大器芯片(均只含有一个运放电路)时工作正常。请问是什么原因导致AD8676烧毁?解决方案是什么?

Parents Reply Children
No Data