AD8021建立时间问题

AD8021的建立时间具体是多少,在Datasheet上The AD8021 is a well-behaved amplifier that settles to 0.01% in 23 ns for a 1 V step. It has a fast overload recovery of 50 ns.设计ADG506+AD8021+AD7665,96通道切换,AD8021延时多少后采集

  • 0
    •  Analog Employees 
    on Apr 12, 2018 12:57 PM over 2 years ago

    AD7665是16位ADC,需要ADC输入信号建立到0.0015%的精度。而AD8021只给了建立到0.01%精度的建立时间为28ns,经验估计建立到0.0015%应该需要40ns左右。

    信号建立发生在ADC转换阶段,AD7665的转换时间t7为750ns。这个时间是很长的,所以AD8021问题不大。需要做的是在处理器给ADC CONVST信号后,立即切换开关,使输入信号在AD8021输出开始建立,等转换结束后,AD8021的输出信号已经ready好进行AD转换。