运算放大器的THD+N参数应该怎样用呢?

大家好,我想给信号采集电路加一级缓冲(同向输入,单位增益放大),需要供电+-12V,压摆率至少20V/us(越高越好)以上。需要缓冲的信号为2MHz以下的单频信号,由于要考虑低功耗并且驱动容性负载,准备评估的双运放芯片有:

ADA4622-2(665uA),ADA4610-2(1.6mA),AD823A(5.1mA),AD8620(3.5mA)以及AD8066(7.6mA)

综合来看ADA8620最优,但是价钱太贵了。准备用ADA4610,但是压摆率又有点低。

我看了这几个芯片的THD+N指标,发现在80kHz以及100kHz以上,都恶化特别明显,在100kHz以上一般为0.01%。仅有AD8066在1MHz时有80dbC,但是AD8066容性负载驱动力不强。由于需要缓冲的是高精密度的信号,频率可到1MHz。我想请问大家:

1、运算放大器的THD+N指标应该怎样用呢?是不是说100kHz的信号通过运放,噪声基地就会抬高到信号能量的0.01%,也就是说信噪比恶化到了40dB呢?

2、运放的THD+N指标是不是和运放的带宽有关呢?

谢谢大家!

Parents Reply Children
No Data