Post Go back to editing

利用CN0385参考电路实现1MHz激励物体表面电压的精确测量

大家好,我想利用1MHz,500uA的电流激励于物体,测量物体表面两点间的电压。我参考了CN0385电路,使用AD8251进行差分转单端,利用LTSpice进行了仿真,见下图:

由于Vp和Vn端具有较大的共模信号,并且共模信号的频率也较大,典型应用下频率为1MHz。但是仿真的结果惨不忍睹,见下图:

我不知道为什么Vp和Vn也失真了,而OUT出来的信号直接被拉到了-5V左右。我想请问下大家

1、对于1MHz下,需要采集的差分信号被淹没在较大共模信号下时,应该怎样设计电压拾取(测量)电路呢?

2、怎么改进CN0385这个参考设计,使得能够采集1MHz左右,且可能有较大共模电压的差分信号信号呢?

谢谢!