AD8332的最大可变增益放大倍数只有20dB

我用AD8332做可变增益放大,采集超声信号,但是目前电路对信号发生器输出的3MHz正弦信号(10mV)实现的最大放大倍数为20dB左右,该增益是可以变化的,放大倍数在1~20dB范围内。

但是实际上AD8332至少自带一个19dBLNA前置低噪声放大,目前我们电路最大才实现20dB的放大,看起来这个AD8332自带的LNA前置低噪声放大的19dB一点效果都没有,各位大神能否帮忙看一下电路原理图,谢谢!

HP_O9和HP_O10是原始信号输入,OP_GAIN是增益信号的输入。

测试电路时,增益信号由一个直流电源提供,范围为0.5~1V。

Parents Reply Children
No Data