Post Go back to editing

关于HMC565LC5电源供电问题

HMC565LC5放大器器件手册上建议不超过+2.5V~+3.5V内供电,如果我用LDO稳出+5V,通过串联两个并联0603电阻,R1和R2,阻值为80欧姆,在放大器线性工作区内(未饱和),那么根据HMC565LC5手册,工作电流按照50mA计算,则到器件供电引脚出电压应为V=5-80*80/(80+80)*0.05=3V ,假想实际工作也按照上诉一样,请问,这样设计方法可以吗?会不会对放大器有损伤的隐患?我们总工说,当器件刚上电瞬间,电流未达到50mA,可能很小,那么压降在R1和R2上的电压几乎为0,那么到放大器供电引脚出电压几乎为5V?这个说法我赞成,但是我的疑问是这可能会对放大器造成损伤吗,因为放大器手册规定供电电压最大为+3.5V?个人认为,手册上给的是稳定供电最大只能+3.5V,否则可能造成器件的永久损伤。想请教一下放大器方面的专家,此设计方法会不会有隐患!不尽感激!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.