AD8276烧了好几个了,照着说明书接线的,求解啊

AD8276的IN+和IN-接在电阻两端,ref和Vs-接地,Vs+接24V,out和sense短接不过为了方便焊把8脚NC和7脚VS+锡点在一块了因为MSOP(RM-8)脚太小了,锡不容易点上,不知道是不是这个原因,另外所接电阻位于100mA的恒流中,阻值为151Ω,两端电压为15.37V(未接入AD8276时所测)。接下来出问题了,当把AD8276的2、3脚引出线接在电阻两端时一切正常,out出来的是15.37V,但是万用表刚接在电阻两端想看看电压是多少时,AD8276烧了。这种情况出现了两次,万用表档位在20V档位,,确认过没有虚焊。烧坏的8276发现IN-,sense,Vs-是短路的。我的疑问是:8引脚和7焊一块会影响么,8276在哪些情况下会烧,在IN-,IN+前面各加一个电阻再接入会不会有用?真的很着急毕竟坏了好几个了,也不便宜。而且这个差分采压不搞定,接下来的电路没法做芯片正面刻字是H1Q,买的型号是AD8276BRMZ。急求大神来解决啊!

Parents
  • 已经基本确定原因了,师兄之前这个电路用这个采样,我以为我改了电路以后可以接着用,其实每通道输入电压变大了就不可用了。说明书里说了每通道最大电压是40-Vs,那么我用的24V电源后就是每通道最大16V。所以也能解释为什么12V可以,17V会烧。现在我的IN+最大22V,而IN-不变,所以out最大为20V那么按照那个电压限制,AD8276是不可能满足了。这几天调试让我明白了别人用过的不能照搬,还有就是说明书一定要看仔细!!!希望大家能从中吸取教训,还有非常感谢各位的热心回答

Reply
  • 已经基本确定原因了,师兄之前这个电路用这个采样,我以为我改了电路以后可以接着用,其实每通道输入电压变大了就不可用了。说明书里说了每通道最大电压是40-Vs,那么我用的24V电源后就是每通道最大16V。所以也能解释为什么12V可以,17V会烧。现在我的IN+最大22V,而IN-不变,所以out最大为20V那么按照那个电压限制,AD8276是不可能满足了。这几天调试让我明白了别人用过的不能照搬,还有就是说明书一定要看仔细!!!希望大家能从中吸取教训,还有非常感谢各位的热心回答

Children
No Data