请问ADI专家老师,
ADA4961、AD8352是否 支持覆盖低频段,如100kHz~10MHz?
我看到datasheet里面性能测试曲线都才到10MHz,但是我的应用需要支持到100kHz。
如果 ADA4961、AD8352不支持10kHz,请推荐一下运算放大器或则RF放大器芯片。
需求:频段0.1MHz~1GHz 功率增益15dB
请问ADI专家老师,
ADA4961、AD8352是否 支持覆盖低频段,如100kHz~10MHz?
我看到datasheet里面性能测试曲线都才到10MHz,但是我的应用需要支持到100kHz。
如果 ADA4961、AD8352不支持10kHz,请推荐一下运算放大器或则RF放大器芯片。
需求:频段0.1MHz~1GHz 功率增益15dB
二者支持100kHz ~10MHz,
如果是RF应用,可以考虑使用RF功放
http://www.analog.com/cn/products/amplifiers/rf-amplifiers/power-amplifiers.html
谢谢您的回答!
RF功放没有能覆盖0.1MHz~10MHz的哦,
您说运放可以覆盖0.1MHz~10MHz,但是测试曲线并没有给出,是否线性度OIP3在低频会恶化比较严重?
产品线的工程师回复如下
The ADA4961 is designed to be AC coupled, and it's gain increases below 10 MHz. For applications that need flat frequency response near or below 10 MHz, it'll be better to use completely dc-coupled, low-distortion differential amplifiers such as
-- ADL5565 Single-channel, 6 GHz diff ADC driver,
-- ADL5566 Dual channel, 4.5 GHz diff ADC driver, &
-- ADL5567 Dual channel, 4.8 GHz diff ADC driver.
Full details for these parts can be found at: