运放输出自激问题

大家好,我在使用AD620和OP284组建的应变桥式微小信号放大电路应用中(使用AD620将微小信号放大100倍,再使用OP284组成反相放大器放大5倍,最后使用OP284做跟随输出),发现在运放OP284输出端接约30米长电缆后采集到的数据带有一个自激噪声,噪声频率500KHz-1MHz之间,幅值约200mV(峰峰值)。运放输出电路如下,不知是什么原因造成的,期望得到您的回答,谢谢

输出电缆长度约30米,非屏蔽非双绞,调试过程如下:

1)C16为10pF时,OUT1处叠加一个频率1MHz,幅值约200mV的自激干扰;

2)将C16增大,比如修改为1000pF,自激现象没有消除,但自激信号的基频约500KHz,并且叠加有更高的频率成分;

3)将R1C接OUT1的连接点修改连接到U12B的输出7脚,并修改输出串联电阻R19的大小为100欧姆,240欧姆,干扰没有改变。

Parents Reply Children
No Data