Post Go back to editing

用AD623搭建了一个电桥信号放大的模块,但是输出不稳定

如图所示,我将电桥的两路输入信号输入,输出一个放大信号在经OP07进行放大,实际PCB焊好调试时发现,总的输出会有一个漂移,而且这个漂移很诡异,有时候会缓慢的增大,而且漂移的时间会很长,几个小时后都还在变化,但速度已经非常的慢,有时候会缓慢的减小,总之就是不能稳定下来,对于放大的信号是IN+和IN-都是2.5V左右,两个之间的差值是零点几个毫伏,输出信号的值主要在mv级跳变,但是由于其总是朝着一个方向漂移,所以一段时间后的累积变化会相对较大,所以不知道大家有没有什么解决方法呢?

Parents
  • 您好,我一共调试了两块电路板,两块原理图都是一模一样的,唯一的区别在于,一块用的是AD622,一块用的是AD623,之前说的AD623的电源电压是超过极限值的,但是AD622并没有超过极限值正负18V,而且之前说的输出不稳定的情况同样出现在AD622上,主要的表现有两个,第一个是偶尔会出现当天第一次上电的时候,他的输出值偏移的比较快,我用12位的ADC来采样,会在一个小时之内偏移20个左右的LSB,但是之后就比较稳定了,第二个就是正常情况下,在达到稳定的情况下,关闭电源,一段时间后再打开电源,大部分实验结果都会在半个小时之内慢慢偏移5个左右的LSB,就会达到基本稳定,后面的变化就会十分缓慢。关于上述的情况,想请问您,我该如何解决这些偏移呢?实际的电路上面已给出,关于供电电源用的是电源模块A2412S转开关电源的24V为正负12V给AD622的。希望能您能帮助我,这个问题已困扰了我很长时间。

Reply
  • 您好,我一共调试了两块电路板,两块原理图都是一模一样的,唯一的区别在于,一块用的是AD622,一块用的是AD623,之前说的AD623的电源电压是超过极限值的,但是AD622并没有超过极限值正负18V,而且之前说的输出不稳定的情况同样出现在AD622上,主要的表现有两个,第一个是偶尔会出现当天第一次上电的时候,他的输出值偏移的比较快,我用12位的ADC来采样,会在一个小时之内偏移20个左右的LSB,但是之后就比较稳定了,第二个就是正常情况下,在达到稳定的情况下,关闭电源,一段时间后再打开电源,大部分实验结果都会在半个小时之内慢慢偏移5个左右的LSB,就会达到基本稳定,后面的变化就会十分缓慢。关于上述的情况,想请问您,我该如何解决这些偏移呢?实际的电路上面已给出,关于供电电源用的是电源模块A2412S转开关电源的24V为正负12V给AD622的。希望能您能帮助我,这个问题已困扰了我很长时间。

Children
No Data