Post Go back to editing

用AD8206做无刷电机相电流检测,很容易出现烧毁的情况!求解!

用AD8206做无刷电机相电流检测,很容易出现烧毁的情况!

做一个无刷控制系统,要求检测相电流,采用AD8206实现,并实现电流保护。系统电源电压要求是50V,设计的持续电流200A,瞬间电流600A为保护点;电路采用手册中典型的应用接线;实际做完板测试时发现,在电源电压40V左右时很容易出现烧毁的情况,烧毁的现象是,IN+,IN-都对地阻值降低,VREF引脚对地阻值也降低,有时还出现VREF引脚直接与地短接的。。。另外,用手触摸IC也会出现坏的情况;总之感觉这个IC很容易就出现损害;具体原因的不明白;IC是找代理商拿的的,看包装应该不会是假货,都是ADI样品包装的;

附件是部分图纸。

attachments.zip