Post Go back to editing

关于I-V转换输出电压出现谐波问题

现有一个微电流放大电路,具体电路见附图,采用运放反馈电阻完成IV转换,输入电流量级约为100nA左右,运放选择AD8512,输入偏置电流约20pA,反馈电阻取值为5Mohm。对电路噪声进行测试时,电流输入端悬空,测试输出端电压及其频谱,频谱中出现了比较大的谐波,但是不知道这些谐波是哪里产生的?是运放的输入偏置电流噪声产生的吗?同时,当把反馈电阻换成1K时,频谱质量很好。我们的放大希望带宽达到150K左右,所以反馈电阻两端不能并联较大电容来限制带宽。尝试在Rf两端并联5pF电容后,整体噪声是降低了,但是谐波还是比较明显。I-V转换电路中,当反馈电阻取值较大(>1Mohm)时,为什么输出电压中会出现明显的谐波?该如何消除这些谐波?是不是器件AD8512的电流噪声引起的?希望高手解答!

attachments.zip
Parents
  • 您好!

    看了您发过来的测试结果,不像是谐波信号。应该就是噪声与杂散信号。应该就是使用了较大阻值的反馈电阻导致的。由于阻值较大的电阻热噪声会比较大,因此建议您换用小阻值电阻。此外,在IV转换时,也建议使用偏置电流较小的运放芯片,如AD549。

Reply
  • 您好!

    看了您发过来的测试结果,不像是谐波信号。应该就是噪声与杂散信号。应该就是使用了较大阻值的反馈电阻导致的。由于阻值较大的电阻热噪声会比较大,因此建议您换用小阻值电阻。此外,在IV转换时,也建议使用偏置电流较小的运放芯片,如AD549。

Children
No Data