请教测高阻器件电压AD8512

工程师们,你们好!我想做的是一个测量高阻器件上电压的电路,测量DC电压,器件阻抗大约是在几百兆。第一步做的是跟随,用的是JFET高输入阻抗的AD8512. 电路如图。但是问题是当正向输入端接上这个100M的电阻时,会降低输入阻抗,这个无法接受。不接这个100M电阻的时候,由于没有给正向输入端提供偏置电流,输出值会锁在一个较大的电压值上,这个输出也无法接受。有没有一种办法,可以使不接测试器件时,使输出接近于0,接上测试器件时,输出就是器件的输出?我知道这不是运放的问题,请ADI的工程师们不吝赐教,谢谢。

Parents
  • 其实不是一定要在运放这边处理来实现您说的输入悬空时,让buffer的输出为0. 可以在电压表这个系统中的其他模块中实现该功能,比如,放大器后面可以加比较器之类的判断器件,当运放被锁定在很高输出值的时候,就认为输入悬空,这时可以强制后面的ADC等输出0.

Reply
  • 其实不是一定要在运放这边处理来实现您说的输入悬空时,让buffer的输出为0. 可以在电压表这个系统中的其他模块中实现该功能,比如,放大器后面可以加比较器之类的判断器件,当运放被锁定在很高输出值的时候,就认为输入悬空,这时可以强制后面的ADC等输出0.

Children
No Data