关于AD8221问题

我用的是AD8221对信号进行放大,其中+V接的是+5V电压,-V接的地,Rg两端的电阻接的51欧姆(相当于放大了900倍左右),当输入端的电压为3.5mV的时候,输出电压为1.578V,当输入端变为3.9mV的时候,输出电压还是1.578V。
当在AD8221输入端加(电阻为1K,电容为2.2UF)低通滤波器时,滤波器之前的电压由1.1mV变化到1.6mV,经过滤波后的电压为2.7mV变化到2.8mV(即AD8221两端的输入电压),而输出电压(放大900倍左右)一直都是2.51V保持不变,一直找不出原因来,有哪位高手知道的请指点下,小弟感激不尽!