Post Go back to editing

If we develop an ATE test card now, from the perspective of supply availability and design complexity, is MAX9979 still the first choice? What about the ADATE3XX series? Which one would be the primary choice for our development?

Thread Summary

The user is comparing the MAX9979 and ADATE3xx series for an ATE test board. The MAX9979 supports -1.5V to +6.5V, while the ADATE3xx series supports -2V to +6V (ADATE302-02, ADATE305, ADATE318) or -1.5V to +4.5V (ADATE320). For 5V functional and 12V stress testing, ADATE318 is recommended due to its dual channel, 1.2Gbps speed, ±25mA active load, and VHH up to 13.5V. If lower power is needed, ADATE305 is suggested.
AI Generated Content
We're currently working on an ATE test board for automotive-grade chip IO testing. We're in the process of selecting a PE (Pin Electronics) chip and would like to compare the MAX9979 with the ADATE3xx series:
  1. What are the differences in positioning and specs between the two?
  2. Which one is better suited for 5V/12V digital pin testing?
  3. Are they pin-to-pin compatible? How are the supply and lifecycle status?
Could you please take a look and recommend which one to go with? Thanks!
    •  Analog Employees 
    on Nov 1, 2026 10:10 AM Contains AI Generated Content
    +1

    MAX9979 is still in Production with no discontinuation notice, ADATE302-02 and ADATE305 are also in Production, and ADATE318 and ADATE320 are recommended for new designs. None of the ADATE3xx parts is pin-to-pin compatible with MAX9979, since the packages, supply rails and register maps are all different. None of these devices drives 12V on the high-speed DCL driver: the driver range is -1.5V to +6.5V on MAX9979, about -2V to +6V on ADATE302-02, ADATE305 and ADATE318, and -1.5V to +4.5V on ADATE320, while 12V comes from the separate VHH output (up to 13V on MAX9979 and 13.5V on ADATE302-02/305/318). If your 12V requirement is a static level, a programming pulse or a stress voltage, VHH covers it; if you need 0V/12V switching at pattern speed, an external high-voltage driver is required. For a new board with 5V functional test and 12V stress, we recommend starting with ADATE318 (dual channel, about 1.2Gbps, ±25mA active load, VHH 0V to 13.5V, on-chip calibration, 1.1W per channel), or ADATE305 if 250-500MHz is sufficient and lower power (0.9W per channel) matters.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.