Post Go back to editing

ad8065450mV

Thread Summary

用户使用AD8065AR实现反相加法器时遇到30mV噪声问题,噪声频率约为290kHz。问题可能源于板上的开关干扰被放大,而非运放自激。建议逐路检查输入路径并保持噪声增益不变,同时重新计算并调整反馈电容Cf的值。
AI Generated Content
Category: Hardware
Product Number: AD8065AR, AD8065

各位专家,你们好!

我们使用了ADI的放大器AD8065AR来实现一个反相加法器,将4路输入按照给定权重相加在一起,再反相输出。同样的电路我们已经是使用了很长时间,也在产品的不同版本上采用。这次是在最新的产品上出现了问题。问题具体表现为加法器输出基线上叠加了噪声载波,该噪声厚度大概30mV(即在基线附近上下跳动范围是30mV左右),该噪声不属于标准的正弦波。如下图所示,图中绿色为之前版本正常的输出基线,紫色为这次出行问题的基线。

我们仔细检查了电路,原理图一样,pcb布局布线基本相同,这种 突然出现的增大噪声是属于什么性质?自激吗?

我们尝试断开加法器输出下一级,问题依旧。给加法器反馈电阻并联一颗2.2pF电容(参考手册)问题依旧。移除所有4颗输入Rg后,问题消失了。请问是否有和方法解决此问题?

Parents
    •  Analog Employees 
    on Sep 22, 2026 11:00 AM Contains AI Generated Content
    0

    紫色那条是周期约3.4µs(约290kHz)的准周期波形,不是随机噪声;这个频率远低于AD8065自激时通常出现的几十到几百MHz,而绿色的正常板上也有同样节奏、幅度小约5倍的起伏,所以更像是板上已有的开关干扰被加法器的噪声增益放大,不是运放自激。

    移除4颗Rg同时断开了注入路径、又把噪声增益1+Rf/(Rg1∥Rg2∥Rg3∥Rg4)降回1,因此不能据此判定自激。建议一次只拆一路、并在求和节点补一颗等值电阻到地以保持噪声增益不变,即可看出干扰从哪一路进来,同时对照板上DC-DC的开关频率是否落在250~350kHz。

    2.2pF偏小:AD8065输入电容共模2.1pF、差模4.5pF,加上PCB和4路走线后求和节点常超过10pF,而MT-059的算例中Rf=500Ω、节点电容20pF时需要5.6pF,请按实际值重算Cf。另外打开示波器的20MHz带宽限制,若290kHz仍在而峰顶毛刺消失,说明低频干扰和高频振铃是两个独立问题。

Reply
    •  Analog Employees 
    on Sep 22, 2026 11:00 AM Contains AI Generated Content
    0

    紫色那条是周期约3.4µs(约290kHz)的准周期波形,不是随机噪声;这个频率远低于AD8065自激时通常出现的几十到几百MHz,而绿色的正常板上也有同样节奏、幅度小约5倍的起伏,所以更像是板上已有的开关干扰被加法器的噪声增益放大,不是运放自激。

    移除4颗Rg同时断开了注入路径、又把噪声增益1+Rf/(Rg1∥Rg2∥Rg3∥Rg4)降回1,因此不能据此判定自激。建议一次只拆一路、并在求和节点补一颗等值电阻到地以保持噪声增益不变,即可看出干扰从哪一路进来,同时对照板上DC-DC的开关频率是否落在250~350kHz。

    2.2pF偏小:AD8065输入电容共模2.1pF、差模4.5pF,加上PCB和4路走线后求和节点常超过10pF,而MT-059的算例中Rf=500Ω、节点电容20pF时需要5.6pF,请按实际值重算Cf。另外打开示波器的20MHz带宽限制,若290kHz仍在而峰顶毛刺消失,说明低频干扰和高频振铃是两个独立问题。

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.