Post Go back to editing

ADA4522-2供电问题

我现在使用ADA4522-2搭建了一个仪表放大器电路,我的输入信号范围是0-5V,所以我选择了ADA4522-2。

规格书上说明供电电压要高于输入电压,我测试使用±5V供电,输入电压在3.5V以上,输出就开始不准了,与规格书说明的一致。

所以我将电源更改为正电源+12V,负电源-5V,经过测试发现在输入在4V以上时,输出也开始不准了。我通过调节正电源的电压,调节到20V的时候,有问题的现象仍然存在。

所以问题1:ADA4522-2的正负电源必须要对称吗,手里暂时没有匹配的负电源,还没有办法验证。

问题2:在输入量程以内,我发现输出的信号会随着正电源的升高而升高。比如我输入信号2V,正电源9V,仪表放大器电路输出在2000uV,此时将正电源修改为12V,仪表放大器的输出变成了2200uV。这是什么原因导致的。

Parents Reply
  • 您是有我们FAE支持的,所以技术问题还请询问他们。我个人的意见是

    1、供电电压可以不对称,输入范围应该在V-到V+ - 1.5V之间

    2、ADA4522的PSRR可以高达150dB,不应该有这么大变化。可接一个电压跟随器看看,如果供电电压变化,输出不变化,那么可能是外部电路问题。建议检查仪表放大器输出参考点(REF引脚)是否被高阻源驱动,或者有电流通路(比如电阻)与电源相连;若是,改为用低阻缓冲(例如一个运放缓冲基准电压),以提高PSRR

    3、另外我们有仿真文件提供,可以按照您实际电路图在LTSpice里面仿真

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.