Post Go back to editing

LTC1966输入隔直电容多大合适?

Thread Summary

The user is designing a circuit to measure the RMS value of a sine wave signal (0-1V, 10Hz-1000KHz) using the LTC1966 with R1=R2=100KΩ and VDD=5V. The final answer suggests an input impedance of 8MΩ and recommends a Cc value of 22nF. Accompanying answers clarify that achieving 0.1% precision across the entire frequency range is challenging, especially at higher frequencies, and suggest using a higher Cc value (22uF) for better low-frequency performance. The user also inquires about the input impedance equivalence and the feasibility of using AD637 for lower power consumption in a 4-20mA application.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC1966

上图是从LTC1966规格书里面摘录出来的,我现在的设计和该图一致,R1=R2=100K,VDD=5V,但是不Cc不知道该如何选?我现在要求测量10Hz-1000KHz,峰值电压为0-1V以内的正弦波信号的有效值,精度希望能达到0.1%,担心Cc太小会导致低频误差增大,请给我下设计规范。

Parents
  • 1.在10Hz~1000KHz范围内实现0.1%的精度不太现实,对于低频部分精度可能会稍好一点,但是当频率上升到几十KHz以上时,LTC1966的精度将会出现下降。

    2.关于Cc电容选型,Cc和内部阻抗组成了高通滤波器。输入的阻抗Req=R1//R2,考虑最低频率为10Hz,准确度为0.1%,由此算出约为7.1uF。考虑到一定的冗余,建议选择22uF或以上阻值的电阻。

    3.如果想追求更高的精度,建议对不同的输入信号的频率使用不同的电阻,您可以参考部分万用表的内部电路,例如吉时利2000这类万用表,其内部使用AD637作为RMS转换器,并根据频率切换不同的输入电阻,实现更高的精度。

  • 1. 设计频率范围为10-1000Hz;2. 电阻分压网络R1和R2接在IN2,为啥会等效成IN1的输入阻抗?3. 我的应用速度有效值测量:ADXL1002 + 积分器 + LTC1966 + 4-20mA驱动电路,功耗允许使用AD637吗?

  • 输入阻抗应该是8MΩ,以此计算出Cc可以选择为22nF。

Reply Children
No Data