Post Go back to editing

AD9914

Thread Summary

The user is unable to synchronize the SYNC_CLK across three AD9914 devices due to insufficient drive capability. The final answer suggests that the issue has been addressed in a related thread, and the accompanying answer mentions using a 2.8 GHz REF_CLK from the ADF4377 to provide a common reference to the AD9914 devices.
AI Generated Content

I’m trying to synchronize SYNC_CLK across three AD9914 devices. I’m using an AD9513 to provide the SYNC_IN signals, and I’ve already achieved same‑frequency, phase‑aligned SYNC_IN to all three chips. I also perform a common DAC calibration and IO_UPDATE for all three parts.
However, I cannot use SYNC_CLK because its drive capability is too weak. With my current setup, I’m still unable to get the SYNC_CLKs on the three DDS devices to be synchronized. What could be the possible reason? And is it possible to achieve this synchronization if I don’t use SYNC_CLK as a reference?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.