@ALee687
如图所示的恒流源电路,只有去掉两个BAV199已经将ADHV4710的开环增益改为1(跟随器模式)才能有±1A的横流输出,如果开环增益增大输出电流就会被钳位,这是什么原因?
@ALee687
如图所示的恒流源电路,只有去掉两个BAV199已经将ADHV4710的开环增益改为1(跟随器模式)才能有±1A的横流输出,如果开环增益增大输出电流就会被钳位,这是什么原因?
感谢回复,但是这里我有个疑问:同样的电路,我用ADHV4702+MOS管的方式就是正常工作的,这整个电路是基本照搬之前的电路,改了放大器而已(用ADHV4710可以去掉两个MOS管)
感谢回复,但是这里我有个疑问:同样的电路,我用ADHV4702+MOS管的方式就是正常工作的,这整个电路是基本照搬之前的电路,改了放大器而已(用ADHV4710可以去掉两个MOS管)
在这个应用里我实际需要的是单位增益就好了。就这个应用来看,您这边更推荐4710还是4702的方案? 我最低电流档需要到10nA,最高电流档是1A.
4710不需要增加额外的管子做驱动,集成度是更好的。
10nA到1A的动态范围还是比较大的,建议通过切换shunt电阻的方式进行挡位切换,这样可以把放大器电路的增益固定住。