Hello, I purchased the EVAL-AD5522EBDZ evaluation board developed by ADI Company. I hope to use it for parameter testing of semiconductor devices. My current device is a three-port device. How should I connect the DUT end of the AD5522 evaluation board? Looking at the previous cases, they all involved measuring the characteristics of resistors. All that was needed was to simply insert a resistor between the two ends of the RDUT. But how do we connect a three-terminal device to be tested?
At this stage, is it possible to use the AD5522 evaluation board to test the IDVG characteristic curve of a MOSFET with three terminals (gate, source, and drain)? Connect the gate to -5V to +5V voltage, the source to 0V, and the drain to a fixed voltage of 0.1V. Then, use the pressure-measurement current (FVMI) method to measure the drain current id, thereby achieving the IDVG test? I saw a blogger who used this evaluation board to conduct the IV characteristic test of a photodiode. So, can this be applied to my three-terminal transistor? I'm currently unsure how to connect the device under test (DUT). Could you please provide me with a clear diagram for the connection? It will be convenient for me to carry out the corresponding operation.Thank you.