此处为什么是要使ADC引脚保持在0.1V以上,需要200mV共模电压。
0.1V是怎么算出来的?
主要问题是要求0.1V以上时,对用的200mV工模电压是如何计算出来的?
ADC要求100mV,所以选择200mV。
“The 200 mV common-mode voltage is required to keep the ADC input pins greater than 0.1 V. ”
如果只有200mv共摸电压,无其他输入,那么ADC的输入是多少?能否算出来
如果只有200mv共摸电压,无其他输入,那么ADC的输入是多少?能否算出来
下图,如果thermopile没有信号,那么ADC1/ADC2为200mV。