Post Go back to editing

AD8334内部衰减器/放大器异常,控制GAIN以后最终VOH的输出不符合预期

目前在项目中采用AD8334对输入信号进行放大增益控制,发现一个比较异常的问题。当输入信号经过AD8334 第一级后测量VOH/VOL实际的输出信号并没有得到预计的放大效果,想寻求一下技术支持 看问题是发生在哪个地方。  硬件设计上将AD8334MODEHILO脚设置拉低,器件增益控制斜率为正,增益控制曲线为4.5 dB to +43.5 dB in LO gain Mode,当我们对AD8334INH输入端输入32mVpp正弦信号, 并对增益控制引脚GAIN输入330mV的电平,此时按照芯片描述经过19dB LNA-33.5衰减器、21dB+3.5dB的后置放大,计算可得GAIN (dB) = 50 (dB/V) × VGAIN 6.5 dB = 50*0.33-6.5=10dB, 那么最终VOH/VOL输出应该放大10dB,但测量输出的VOH/VOL结果并没有得到相应放大,我们逐步测量下来发现32mVpp信号从INH进入并经过LNA到达 VIP/VIN 时正弦信号为292mVpp,放大了19dB,符合预期。但当292mVpp进入VIP/VIN后级的0~-48dB ATTENUATOR21dB+3.5dB的后置放大器后输出结果仅为46mV,实际只增加了3.2dB,是否还有其他因素影响LNA后端的ATTENUATORPA。下面是我们设计的简易框图

Parents Reply
  • 原理图是通道1的输出进通道2的VGA,通道2的LNA没用。通道3和4同理。

    以通道1和2为例,建议去掉R6R8C12C15, 即只调通道一,看是否正常。

    另,INH2和INH4,我看你是直接接地的。认为不妥,INH脚芯片内部接的是3.25V的直流偏置,如果外部接地,相当于将3.25V短路到地。

Children