CN0267_CN中
CN0267 设计和集成文件中
请问以哪个为准
CN0267_CN中
CN0267 设计和集成文件中
请问以哪个为准
您好,根据芯片手册,"Under normal operating conditions, the voltage between COM and LOOP− does not exceed 1.5 V, and the voltage at LOOP− is negative with respect to COM. If it is possible that the voltage at LOOP− may be forced positive with respect to COM, or if the voltage difference between LOOP− and COM may be forced in excess of 5 V, a 4.7 V low leakage Zener diode should be placed between COM and the LOOP− pin, as shown in Figure 50, to protect the AD5421 from potential damage." 因此,阴极接地以避免该点电压低于-5V(Com为0V)。