LTC6268-10这一款芯片作为跨阻放大器如何去测试?
在LTC6268-10输入端用源表输出一个电流,只焊接增益电阻RF,输出接示波器,去测试他的放大效果
但是一直是噪声,是这种测试方法的问题嘛,还是说输入端只能接光电二极管?
输入的是一个脉冲电流信号,幅值1uA,脉宽500us,得到的是一个噪声
LTC6268-10这一款芯片作为跨阻放大器如何去测试?
在LTC6268-10输入端用源表输出一个电流,只焊接增益电阻RF,输出接示波器,去测试他的放大效果
输入的是一个脉冲电流信号,幅值1uA,脉宽500us,得到的是一个噪声
I think there is too much capacitance and noise on the current source. That board was made to have a photodiode edge-mounted, but I suggest just using an input resistor to change a voltage into a current…
如果你说的噪声是黄色波形的话,是不对的。黄色波形是震荡了。
1.不接输入信号源,测试AMP输出是否有震荡?如果仍然有震荡,那么你得参考DC2414A的布局布线,以及数据手册的关于PCB layout的论述,来重新画PCB。或者购买DC2414A进行测试。
2. 如Glen所说,如果要测试IV电路的性能,不建议直接输入脉冲电流。建议产生一个脉冲电压V,经过一个电阻R后连到AMP的-IN,那么等效的脉冲电流为V…
上图同相输入端,即+端,通过12kohm接地,其实就是接地了。