Post Go back to editing

ADCMP567 应用

Thread Summary

The user inquires about the correct configuration of LE and LEB pins for the ADCMP567 high-speed comparator to achieve hysteresis without latch. The final answer confirms that Figure 10 in the datasheet can be used, with LE grounded and LEB connected to the hysteresis voltage, to implement the desired hysteresis functionality.
AI Generated Content

你好!

   新的产品选用ADCMP567 高速比较器,设计中有个疑问,比较器不需要latch功能,始终处于比较状态,并且需要使用hysiersi功能。按照规格书说明,如果不需要latch,将LE接VDD,LEB接VDD-2.0 即可,若使用hystersis,需要保持LE- LEB 是个负电压,LE和LEB该如何接法,目前使用规格书给出的典型应用电路,LE接地,LEB接hystersis电压,这个电路能正常使用比较功能吗?

  • For the LATCH to be enabled and disabled, the inputs of LE and LEB should be complementary.
    In figure 10, LE is GND but LEB is not VDD and therefore the inputs are not complementary.
    Now as Figure 10 in the datasheet, this configuration will implement hysteresis depending on the differential voltage between LE and LEB.

    所以Figure10 可以实现比较功能,用LEB脚来设置迟滞电压。

  • 你好!这个hysis功能是否要求输入信号是零偏置,输入+端是信号,-端接地。我们现在的应用是+端信号,-端接一个触发电平信号,信号和这个触发电平进行比较,这种应用情况下,还能用这个hysis功能吗?这种应用是否需要按照Figure 7来设计,谢谢!!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.