Post Go back to editing

How to adjust the ADuM4190 EAout2 BIAS

Hello

I want  to use ADuM4190 as a isolater and splitter amp. when a 1V sine signal on IN+ ,I want to use EAout as a output with 1 V/V GAIN and use EAout2 as a output with 2.6 V/V GAIN.

The VDD1 is 5V DC. However the EAout2 output is clamp on 5V. How can I descreas the EAout2 output BIAS to lower voltage?

Thanks