Post Go back to editing

AD8065搭建TIA加负电源轨后震荡

Hi

各位 ADI的老师好,我用贵司的AD8065搭建了跨阻电路,单电源5V供电,增益为1G,调试时使用信号发生器输入脉冲,测试一切正常,当我想改为双电源轨供电,即在2引脚飞线引入-5V后,输出发生震荡,如图2.且整个负电源轨电源系统都被拉低,LDO-5V被拉低了,给LDO供电的负电源也被拉低了,奇怪的是,我在上电以后再手动接入-5V就会正常,真是百思不得其解,怀疑去耦的问题,我还在2引脚加了去耦电容,也没有效果,LDO输出能力500mA,甚至怀疑上电瞬息间带载电源没起来,在运放2角串联100欧姆电阻也米有效果,给电源加软起动也没有效果,请教各位老师,我这个应用,运放加了负电源为什么会出现这个现象呢?

Parents Reply Children