Post Go back to editing

ADA4870的问题

你好,有以下几个问题麻烦解答,非常感谢!

1.我想用ADAD4870做一个恒流1A的压控恒流源,驱动10Ω的负载(这个负载是个假负载即一个电阻),在供电电压±15V的时候是否能实现(散热好的情况下)?详细设计参考的是www.analog.com/.../a-large-current-source-with-high-accuracy-and-fast-settling.html

2.但是这个设计有一点没有明白RO越大功耗越小,但是与图上的数值不符,除了温升还有什么设计时候需要建议的重点吗?

3.ADAD4870显示不推荐新设计使用,是否意味着后续会停产呢,如果是的话有替代型号吗?

Parents Reply Children
No Data