Post Go back to editing

ADA4899减法器偏置调节电路问题

用ADA4899-1运放设计了放大电路最后一级作为偏置调节输出,电路图设计如下 ,  用手动调节模式,即用跳帽盖住J2的2-3管脚,调节R3,使其电路偏置J6为零(没有输入时,调节整个电路的偏置),现在测试无论如何调节R3的值,输出out J6的值一直是1.658V,无论怎么改变偏置调节都是一样的值1.658v,测量R3两端的电压值,是能测量到改变值的,不知道什么原因造成的,麻烦各位工程师帮忙看看,是否电路设计存在问题,同时ADA4899-1做减法器使用时的引脚FEEDBACK是否需要连接到输入端呢,谢谢,麻烦各位帮忙看看呐

Parents
  • 感谢感谢回复呐 同时还想请教个问题我这边有个电路设计关于微弱电流检测的放大电路,里面涉及到了ADI的对数放大器AD8305,压控增益AD8330,偏置调节电路ADA4899,现在有几个问题,想向您请教下:(1)关于AD8305的对数放大器,没有接任何输入,输出Vout(12)引脚是有180mv左右的值,这个是芯片本身的偏置电压嘛 (2)电路中对数放大输出180mv之后经过R24(50Ω)后变成了0.389mv,不知道什么原因,AD8330的输出电压范围是0-2VMAG嘛,引脚VMAG悬空时,GMAG是1嘛,电路测试时,VMAG悬空,VDBS为0.55V,AD8330的输出测试时电压值一直是2.5V不变,想请问下这个是什么原因呐

Reply
  • 感谢感谢回复呐 同时还想请教个问题我这边有个电路设计关于微弱电流检测的放大电路,里面涉及到了ADI的对数放大器AD8305,压控增益AD8330,偏置调节电路ADA4899,现在有几个问题,想向您请教下:(1)关于AD8305的对数放大器,没有接任何输入,输出Vout(12)引脚是有180mv左右的值,这个是芯片本身的偏置电压嘛 (2)电路中对数放大输出180mv之后经过R24(50Ω)后变成了0.389mv,不知道什么原因,AD8330的输出电压范围是0-2VMAG嘛,引脚VMAG悬空时,GMAG是1嘛,电路测试时,VMAG悬空,VDBS为0.55V,AD8330的输出测试时电压值一直是2.5V不变,想请问下这个是什么原因呐

Children