Post Go back to editing

ADA4899减法器偏置调节电路问题

用ADA4899-1运放设计了放大电路最后一级作为偏置调节输出,电路图设计如下 ,  用手动调节模式,即用跳帽盖住J2的2-3管脚,调节R3,使其电路偏置J6为零(没有输入时,调节整个电路的偏置),现在测试无论如何调节R3的值,输出out J6的值一直是1.658V,无论怎么改变偏置调节都是一样的值1.658v,测量R3两端的电压值,是能测量到改变值的,不知道什么原因造成的,麻烦各位工程师帮忙看看,是否电路设计存在问题,同时ADA4899-1做减法器使用时的引脚FEEDBACK是否需要连接到输入端呢,谢谢,麻烦各位帮忙看看呐

Parents Reply Children
No Data