Post Go back to editing

ADHV4702增大输出电流,烧芯片问题

Thread Summary

用户尝试通过使用VP2540和VN2540 MOSFET来增加ADHV4702的输出电流至100mA,但在实验中ADHV4702在输出电流超过50mA时会过热并损坏。最终解决方案建议将R6电阻值减小至10kΩ以减少功耗,并确保MOSFET的栅极驱动和过流保护。此外,建议移除原电路中的Q1和Q2保护电路,以避免仿真中的奇变问题。
AI Generated Content

想把ADHV4702的输出电流增大到100mA, 采用VP2540和VN2540两个MOS管,按照datasheet上的图设计电路。仿真看步到问题。但是,在实验中,ADHV4702大概输出电流50mA超过1分钟就会烧芯片。已经烧了6pcs了,求帮忙

Parents Reply Children