Post Go back to editing

关于AD210这款隔离放大器,其输入端的管教保护怎么做

AD210芯片的16、17、19 这3个PIN,内部有二极管的钳位保护吗? 即:对正15V电源的二极管,对-15V电源的二极管;是否存在?

外部电路应该怎么对管脚进一步保护呢? 

Parents Reply
  • 请帮忙再看一下实际应用电路图。信号输入端AC_IN+和AC_IN-端,有效值4V的交流信号输入

    做浪涌冲击试验,可以到4000V。实际使用过程中,AD210前级损坏,测量表现为前级电源输出不正常,后级电源正常但无输出。断电状态下前级正负电源间电阻为30欧姆左右。

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.