Post Go back to editing

关于AD8367 S2P文件的一些疑问

您好,关于D8367 S2P文件我有一些疑问,以240MHz为例,

1)s2p文件中最大增益文件240MHz附近增益为8.9dB,S11和s22也比较好,请问是否是demo板匹配后的测量结果?

2)该s2p文件对应的demo板是否使用了datasheet fig.42的宽带匹配形式?手册table7上说,使用电阻的宽带匹配形式会引入11.5dB插损,那么输入输出的匹配是不是总共引入了23dB插损呢?

3)如果匹配引入23dB损耗,s2p中S21=8.9dB,那么240MHz附近AD8367的增益则为31.9dB,可datasheet里240MHz gain为43dB,请问这是怎么回事呢?

4)如果我想在500MHz 某点频上用LC做窄带匹配,能否提供一下AD8367去掉匹配电路后的s2p文件呢?