你好,在使用AD8132差分运放仿真时,有以一疑问,烦请解答
1、输入一个0.2Vpp的交流信号,经过电阻以后,怎么只有0.083Vpp?
2、Vocm脚在实际使用时可以悬空吗?
| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Awaiting Customer Response | |
你好,在使用AD8132差分运放仿真时,有以一疑问,烦请解答
1、输入一个0.2Vpp的交流信号,经过电阻以后,怎么只有0.083Vpp?
2、Vocm脚在实际使用时可以悬空吗?
我觉得你需要考虑你的输入信号的源阻抗,是否在电路中形成了分压;
Vocm是不可以悬空的,你必须要要给你的输出一个共模电压,输入你希望输出为-2.5V到+2.5V,那你的共模电压为0,如果是0~5V,则你的共模电压为2.5V!
1、以上数据是通过仿真软件得来的(见上图),输入VinP=0.2Vpp,信号源内阻为1.71K,通过Rg=1K后,变成了0.083Vpp,也就是Vp=0.083Vpp,就是就是Vp不知道0.083Vpp是怎么计算的?
2、Vocm在中电流的电流为12mA(这个典型值),是不是意味着在给脚时,能保证脚的电流达到手册中电流的要求?
LIHAI