Post Go back to editing

AD8628和ADA4505的几个问题,小白提问

1.请问AD8628的供电,可以采用V+接+5V,V-接-5V吗?

红色方框的内容“5 V单电源操作”,意思是必须接5V单电源供电? V+接+5V,V-接-5V不可以吗?

2. 请问ADA4505的供电,必须是“1.8 V至5 V单电源或±0.9 V至±2.5 V双电源供电”吗? V+接+5V,V-接-5V不可以吗?

注 : 纯新手,手册看不懂,求求各位帮帮忙。

Parents Reply Children