Post Go back to editing

AD8330和AD8138级联中中间有1dB的损耗,是什么原因呢,是需要阻抗匹配么,需要怎么匹配呢

级联中存在好多问题

Parents Reply Children
  • 哦哦,学到了,对于10MHz的正弦信号进行放大,那这两级级联的中间可以直接连接么,还是需要阻抗匹配呀,我就是有些搞不明白级间遇到什么情况需要阻抗匹配,如果要匹配,该怎么匹配?没有搜到实用的资料。

  • 我不确定需要50R的阻抗匹配还是多少,如果是50R,你需要在你的每一级输出端串联一个50R的电阻,相当于从每一级电路单元的输入端往前一级看。如果你的前一级是运放得输出,闭合环路的运放一般视为理想恒压源,理想恒压源内阻无穷小,如果你需要50R阻抗匹配,那就需要在运放的输出端再串联一个50R电阻,这就是戴维南定理的实际应用。