Post Go back to editing

CN0359方案中多个芯片容易被烧毁!

您好!

我想设计一个用于水质电导率测量的小型设备,因为看到你们的CN0359全自动高性能电导率测量系统的宣传性能不错,我购买了评估版并做了几块测试板进行测试验证,发现至少有3块板子(包括购买的原装评估板)发生莫名其妙的故障。最近有空进行了逐一排查,发现几个问题如下:

1、故障电路板-1:原装评估板。上电过程中,D2(1N4148W)出现冒烟,±15V无法输出(L5的3.3V输出正常)。经过排查,发现U15(AD8253ARMZ)的VDD与VSS已经导通!这导致整个电路板的+15V与-15V网络导通!D2一上电就被烧毁!

2故障电路板-2:评估板的复制板。上电后测量±15V无输出。检查发现,(1+15V-15V网络之间已经导通!(2)±15V网络与GND网络导通!疑似有芯片内部烧毁。经过仔细排查,发现

 (1U17ADG1211):VDDVSSGND均处于导通状态!

 (2U13ADA4638-1:V+V-之间导通了!

 (3)更换U17U13后,+15V正常,-15V偏低(-14.887V)。更换U18AD8253ARMZ)后为-14.984V。电路板恢复正常。

3、故障电路板-3:评估板的复制板。上电后,双铂金片电极的其中一极冒气泡(自来水溶液中)。疑似在电极上产生了电解反应。排查发现:

1)电极接线端J514脚断开下故障仍旧出现,表明不是激励电流造成的。

2J5-2脚的电压约-14V!更换U15AD8253ARMZ)后,J5-2的电压恢复正常(约-3.9V),但稍后降为-2.6V。上电后电极不再冒泡。

3)更换与J5-3连接的U14ADA4000-1)后,J5-2的电压还是约-2.6V,但使用1K电阻测量结果为正常。

 

以上的测试条件如下:

1、供电电源:220VAC通过DC5V/3A的直流电源转换适配器给电路板供电。

2、参数设置:

     激励电压:1.0V;激励频率:1.0K Hz;其他参数均使用默认参数。

3、电极:使用过两种类型电极(1)四线制电极,两个银片与激励电流端子连接,两个Ag/AgCl电极与J523端连接,J5-5GND)未连接。(2)双铂金片电极,分别与J51-23-4连接,J5GND未连接。

 

想请教的问题是:为什么这个电路的芯片很容易被烧掉?!特别是AD8253ARMZ。是我的使用存在问题吗?还是电路设计或芯片本身的问题?

希望能得到你们的解答!

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.