使用LTC6561作为TIA,对APD两端加正高压,APD输出正向的脉冲信号,经过LTC6561,信号反向,但是信号摇摆范围只有300mV左右,通过调节Vref引脚电压,也只能调节到500mV的摇摆范围;推荐电路上是对APD两端施加负高压,有没有其他的推荐方式可以实现提升信号摇摆范围,还有什么因素影响反向的信号摇摆范围?
使用LTC6561作为TIA,对APD两端加正高压,APD输出正向的脉冲信号,经过LTC6561,信号反向,但是信号摇摆范围只有300mV左右,通过调节Vref引脚电压,也只能调节到500mV的摇摆范围;推荐电路上是对APD两端施加负高压,有没有其他的推荐方式可以实现提升信号摇摆范围,还有什么因素影响反向的信号摇摆范围?
如果是正高压必须要用交流耦合,因为LTC6561只能sourcing电流,参考下面的电路设计:
提供的参考电路实际上对于LTC6561而言,输入也是反向的脉冲信号,从APD的阴极输出反向脉冲。我想问的是当从APD阳极输出信号,即LTC6561的输入引脚信号是正向脉冲,经过LTC6561,信号反向,此时信号的动态范围,可以通过什么手段调节?
输入正向脉冲,意味着会往LTC6561面灌入电流,这会导致器件工作不正常,LTC6561只能输出电流,无法输入电流,我们不推荐这种用法。