Post Go back to editing

AD8422增益控制

请问大佬,我预想用ADG804来控制AD8422的增益,搭了以上的电路,在无输入信号时,发现在第一级放大输出端P2测得的电压是-4.8V,第二级放大输出端P4测得的电压为-10V达到饱和。

然后我将ADG804的VDD、EN和GND引脚断开后,放大电路输出端为0V。

请问一下这是什么原因造成的?另外想请教一下,有没有除了多路复用器改变电阻之外其他程序控制增益的方法?

Parents
  • 输入不能浮空,浮空会导致很多的不确定性,比如有一个漏电流流入你的AD8422,而AD8422的输入阻抗又很高,可能会导致产生一个不确定的电平。如果你想确定你的增益正常,需要将输入接地。VDD断开后,你的运放不工作,当然信号为0.

    你可以看看我们的可编程增益仪表放大器PGIA,比如ADA4254和LTC6373

Reply
  • 输入不能浮空,浮空会导致很多的不确定性,比如有一个漏电流流入你的AD8422,而AD8422的输入阻抗又很高,可能会导致产生一个不确定的电平。如果你想确定你的增益正常,需要将输入接地。VDD断开后,你的运放不工作,当然信号为0.

    你可以看看我们的可编程增益仪表放大器PGIA,比如ADA4254和LTC6373

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.