ADA4860-1 LTspice单电源5V电路仿真:输出未实现放大功能

双电源±5V供电可实现信号放大

而单电源+5V供电状态,无法实现信号放大,请确认下电路设计是否存在问题

Parents Reply
  • 0
    •  Analog Employees 
    on Oct 27, 2020 2:48 AM in reply to wanwanjin

    ADA4860-1的模型问题,或者说模型建立后,是以+/-5V供电进行测试的,没发现问题。而没有对单电源+5V的情况进行测试,所以模型仿真会有问题。

    实际电路的话,如果输入是2.5V~2.8V,输出也是2.5V~2.8V,输入输出信号都在ADA4860-1的指标范围内,是没有问题的。

Children