AD8138低温需要更高工作电压的问题

        我用AD8138按照手册上的接法做5MHz信号单端转差分给后级AD9238采样。AD9138单电源3.3V供电,交流耦合输入峰峰值500mV信号,常温下输出的2路差分波形正常。做低温试验,发现0度以下,随着温度的降低,波形逐渐失真,到-40度明显失真,AD采样后的数字信号作图看波形像是顶部失真,做FFT后发现谐波变大了,怀疑是饱和了,所以用稳压电源单独给AD8138供电,在-40度的时候给3.3V电源输出失真,将电源提高到3.7V以上后输出就好了,经过对比和常温下一样。现在是直接把板子上的5V给AD8138做电源。

        请问,AD8138在低温下是需要比常温下更高的电源么?我需要就这个现象写个报告,但是不知道机理是什么,麻烦高人指点,谢谢!

Parents Reply Children