关于跨导放大器的使用问题

跨导放大器的输出高阻抗吗?如果想把输出的信号接一个小电阻转化成电压信号直接送入STM32的ADC采集口是否可以?还是输出级要加入缓冲级?

Parents Reply
  • 0
    •  Analog Employees 
    •  Super User 
    on Dec 4, 2019 7:52 AM in reply to Jasper_wang

    OPA615显然不适合做TIA电路,因为其输入的偏置电流过高,典型值为+/-3uA,你的APD管输出如果是10uA那么运放的偏流就会导致你的输出有30%的误差,这显然是不可接受的。从你的选择来看,似乎输入是一个脉冲电流,如果是这样,一定要用低偏流,高带宽的运放,比如ADA4817和LTC6268。运放只要构成反馈,在其输出负载电流内,都等效为内阻无穷小。如果要求不高,完全可以接入MCU的ADC,但是如果ADC是SAR型的,需要更高的驱动电流,或者你需要更高的精度,就需要在ADC前增加差分输入。这完全是基于你的需求而来。

Children
No Data