Post Go back to editing

利用AD5522怎么设计一个正负30V的PPMU?

利用AD5522怎么设计一个正负30V的PPMU? AD5522输出电压最大只能输出正负11V左右。但我们客户的需求是30V的。不知道用AD5522能否设计出30V的ppmu?。如果利用升压电路可以解决,硬件的方案是如何的呢?

Parents
  • Wendy 你好,

    目前ADI内部有个DPS/SMU的参考设计正在进行中,就是基于AD5522来扩压扩流完成+/-50V 5A的四象限电源或PMU、SMU的设计的。AD5522后面加高压运放(LTC6090-5)完成扩压,扩流的话用功率三极管推挽电路来实现的(类似音频功放电路)。但是如果你对电流的需要只要1A以下这种级别的,也可以用ADA4870的扩压电路就可以实现,稍微简单一些。主框图如下。详细支持可以联系我,jay.huang@analog.com

Reply
  • Wendy 你好,

    目前ADI内部有个DPS/SMU的参考设计正在进行中,就是基于AD5522来扩压扩流完成+/-50V 5A的四象限电源或PMU、SMU的设计的。AD5522后面加高压运放(LTC6090-5)完成扩压,扩流的话用功率三极管推挽电路来实现的(类似音频功放电路)。但是如果你对电流的需要只要1A以下这种级别的,也可以用ADA4870的扩压电路就可以实现,稍微简单一些。主框图如下。详细支持可以联系我,jay.huang@analog.com

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.