The AD8274 is specified at ±15 V, but it can be used with unbalanced supplies, as well. For example, −VS = 0 V, +VS = 20 V. The difference between the two supplies must be kept below 36 V
数据手册中这段话不是说明了AD8274在负电压是0V时,正电源小于36V就可以工作吗?,我使用5V供电,输出最小也还有0.8V左右。